Share this
New Classes Offer Hands-On Training For IPT Fittings
by Alecia Robinson on Thu, Apr 13, 2017 @ 11:04 AM
We'll show you how to handle cone-and-thread fittings for higher pressures
The medium and high pressure cone and thread essentials training instructs attendees to identify correct tube system placement, correctly install Swagelok® tube fittings, and troubleshoot other common fluid system mistakes. Find out more about our Swagelok Essentials courses offered at Edmonton Valve & Fitting.
Swagelok's IPT fittings require a different approach than standard Swagelok fittings. For one thing, they use heavy-duty tubing that must be threaded like pipe. Then the end must be coned at a 59-degree angle for a tight fit. To make sure our customers get top performance from these components, Edmonton Valve & Fitting has launched a new series of training classes.
IPT fittings come in two styles, one for medium pressure up to 20,000 psig or 1378 bar, and one for high-pressure applications of up to 60,000 psig or 4134 bar. These cone-and-thread fittings are designed specifically for the oil and gas, chemical, petrochemical, water jet cutting and blasting, and aerospace industries.
Lecture and lab
As with our regular tube-fitting sessions, this training involves three to four hours of classroom instruction and includes the opportunity to practice making an assembly. It's an ideal way for field technicians to get comfortable with the process. It's also a good opportunity for engineers to gain an understanding that goes beyond the specs on a sheet of paper or computer screen.
Because the fittings are designed to work under such high pressures, we don't put the students' work through a burst test as we do in our standard tubing class. But the design of the IPT fitting includes a small weep hole that reveals leaks due to a poor seal. In our class, we include troubleshooting tips for when that happens.
It's also important to cut the proper length of tubing for the job, and we'll show you how to calculate it. It's expensive to waste any kind of tubing, but even more so for IPT tubing, which has walls tp to three times as thick as standard tubing.
Because of the thick walls, the tubing must be treated a little differently. It requires a bigger bend radius. Make too tight of a bend, and you can crack the tubing or even damage the bender.
Because the sealing surface is so small on IPT fittings, vibration can be a bigger problem than normal. We'll explain how to deal with these high vibration applications.
When it's all done, you'll get a certificate of completion.
Here or there
We hold our half-day classes here at Edmonton Valve & Fitting, but we can also provide the training at your site. Contact us at 780-437-0640 or through our website to find out when our next training session is scheduled, or to set up an in-house class.
Additional resources