Freezing Weather's Almost Gone, But It's Not Forgotten

Posted by Alecia Robinson on Thu, Apr 27, 2017 @ 09:04 AM

Start planning for next winter now with our insulation and tracing packages


insulated & heat trace.png

Edmonton Valve is your single source for tracing products, equipment, and training. To find out more about our line download the Pre-Insulated Tubing Bundles Catalogue.


Now that the weather is warming up around Edmonton, it's tempting to forget about the cold-weather hassles we're leaving behind. But you know better. You know that this is the time to start thinking about how you'll make improvements before next winter comers.

Edmonton Valve & Fitting makes it easier because we can be your single-source supplier for heat tracing and insulation packages. It starts with the tubing itself: bare coil tubing, traced tubing, and insulated tubing. We also have pre-insulated tubing, banding and clips, heat transfer compounds, steel tags, heat shrink boots, fluid distribution headers, valves, and of course all the tube fittings and unions you need to complete a job.

A dual stage tube straightener is available for rental to complete your job.  This will help get all the kinks out of any bare coil tubing size. 

Whether yours is a glycol, steam or electrical application, you don't have to go to 10 different suppliers, because this is one area where we go beyond Swagelok's product offerings to make sure you have what you need.

Why worry about this now? Because you need to think about coordinating with your planned shutdowns, facility upgrades and capital projects. Most of our clients go for two to five years between shutdowns. If you need to replace steam lines, proper tracing and insulation can't be a last-minute add on.

Get it right

Components can't do their jobs well if they aren't properly installed. Proper training also increases safety and decreases costs. For people who don't spend a lot of time installing and upgrading tracing packages, such as crews for insulating contractors and construction contractors, it's smart to get a refresher. We're here to help on that score as well.

We offer a full-day class each month on tube fitting installation training, a mix of classroom lecture and hands-on practice. The seminar emphasizes choosing correct tubing and fittings for the site, proper handling, preparing, and installing components to specification. Each participant gets to assemble tubing and fittings, then see how their work holds up under pressure in our burst chamber. Pass the class, and you get a certificate of completion that is ABSA recognized. 

Whenever you need to jog you memory, we also have detailed installation instructions in printed form, with reference photos.

So while you are enjoying the warm weather, make plans to keep everything running smoothly when it turns cold again. Call Edmonton Valve & Filling at 780-437-0640 or contact us through our website, and we can help you put together the insulation and tracing packages that you need.


Additional resources:


 

Topics: winterization, Tubing