ABSA and MTRs: We Have Your Parts Covered Part 2
by Alecia Robinson, on Tue, Sep 12, 2017 @ 15:09 PM
We have documentation for components for systems running at more than 15 psi
Need an MTR for one of your Edmonton Valve orders? Head over to edmontonvalve.com/mtrs to download a copy, all you need is the heat number which is stamped right on your tubing.
As we discussed in an earlier post about ABSA and CRNs, the Alberta Boiler Safety Association is the pressure equipment safety authority authorized by the Alberta Government to administer and delivery safety programs related to boilers, pressure vessels and pressure piping systems through their complete life cycles. In this weeks blog we will discuss how ABSA relates to Swagelok when it comes to Material Test Reports (MTRs).
Documentation
For threaded piping and tubing, ABSA suggests that owner companies have certain procurement and purchasing requirements from its approved vendor list. Although Material Test Reports may not be required by construction code, MTRs may be required in owner specification. So it's up to the owner to train personnel in the MTR verification and other documentation requirements
MTRs and CoCs
Edmonton Valve & Fitting can help out by providing documentation. We provide MTRs for all tubing orders. They are based on the heat number printed on the lay line of the tubing. We also have a self-serve option available for MTRs for tubing online at edmontonvalve.com/mtrs. Simply enter the heat number and you can download the MTR. If you are cutting the tubing, then the heat number should be written onto the tubing
MTRs are typically not provided with other products, but they are available on request. All parts are traceable for alloy materials with a three-letter heat code that is stamped onto all fitting components which meets the ABSA requirement. It speeds up the process if you request the MTR at the time of order. Keep in mind that a tubing tee could have up to 10 MTRs associated with it.
Another commonly requested document we receive is a Certificate of Compliance. We can provide a Certificate of Compliance upon request, just mention this request when speaking to your customer service associate. A CoC will be issued for the entire order, and parts are listed out.
Additional resources
- Need Tubing Material Test Reports? Edmonton Valve Has Them Online!
- ABSA and CRNs: We Have Your Parts Covered
In a hurry or have a question? Please click here to get in touch - we respond fast! Or call 780.437.0640.