Share this
Swagelok Flange Adapters Ease Transition from Pipe to Tubing
by Katie Reid on Fri, Feb 19, 2016 @ 14:02 PM
Simplify the design and save weight compared with threaded branch connections
Interested in more information on Swagelok's Flange Adapters? Download your copy of the Flange Adapter Catalogue.
When a fluid systems operator wants to get information such as pressure, temperature, and flow from a piping system, one common method is to use Thredolet® or Weldolet® branch connections. That strategy may get the job done, but the results can be complex and cumbersome. It's easy to wind up with a multitude of nipples, valves, and other threaded or welded components.
All that added weight is subject to vibrations from the process pipe, increasing the chance of a pipe break, resulting in potential for a dangerous gas leakage. Then production has to be shut down while someone makes repairs; this can make for a costly day at the office.
A better way
Swagelok's flange adapters and modular flanged valves make the job a lot easier. They provide a threadless, weldless transition from flanged pipe to tubing, reducing both the number of connections and the overall weight. They come in several configurations, including flat face, raised face RTJ and tongue-and-groove. They also have wrench flats to ease the assembly of tube fittings.
We were able to implement this type of solution recently for one of our customers, a large energy company that transports and distributes crude oil, natural gas, and other liquids. They had problems with a system of branch connections on a system under 1,440 psi, taking fluid from a process pipe to a pressure relief valve. The heavy assembly created intense vibration. Now, thanks to Swagelok, the customer has a simple, clean connection that takes up little space and doesn't add much weight to the system.
Does your fluid system need a simpler approach to branching off from your piping system? Let someone from our staff show you how to make it happen.
Additional resources
- Those Expensive Tools? You Can Borrow Them from Edmonton Valve
- Edmonton Valve Hosts Local Community Events for Fun and a Good Cause
- Watch for These Sampling System Mistakes That Can Hurt Your Operations
In a hurry or have a question? Please click here to get in touch - we respond fast! Or call 780.437.0640