Minimizing Mechanical Seal Leak Rate in Your Alberta Facility
by Thomas Webster on Fri, Sep 09, 2022 @ 08:09 AM
The extent of loss from a mechanical seal support leak rate can vary, but they’re inevitable. One major reason for pumping application failure, as seen across refineries in Alberta, has been mechanica …
How SAGD Subcool is Affected by Fluid Dynamics
by Thomas Webster on Tue, Sep 06, 2022 @ 09:09 AM
Recovery of heavy oil in steam-assisted gravity drainage (SAGD) is highly dependent on the temperature and viscosity of the fluids involved. It is well established that when the heated steam is passed …
Top Refinery Emission Factors and Source Mitigation Strategies for Alberta Plants
by Thomas Webster on Fri, Jun 03, 2022 @ 08:06 AM
Refineries are one of the largest sources of energy and are important to accommodate the ever-growing energy demand of the modern world. However, refinery emissions are often high and include air and …
Ensuring Smoother Oil and Gas Operations in Fort McMurray Canada
by Thomas Webster on Fri, May 27, 2022 @ 08:05 AM
When it comes to oil and gas operations in Fort McMurray, Canada, equipment reliability is key. For heavy oil and bitumen transport, there needs to be confidence that your equipment can stand up to th …
Top Strategies for Refinery Winterization in Edmonton’s Process Plants
by Thomas Webster on Thu, Apr 21, 2022 @ 16:04 PM
Controlling ambient parameters is central to ensuring a fluid system is running smoothly. If a drastic change in temperature occurs—and isn’t planned for—it can amplify the harmful effects of the flui …
How To Optimize Your Fugitive Emissions Plan in Edmonton Refineries
by Tristian McCallion on Wed, Jan 12, 2022 @ 09:01 AM
Fugitive emissions are the bane of any refinery process. Releasing methane contributes to intensifying climate change effects and is twenty to forty times more effective at trapping heat than an equal …