How to Maintain Hydrogen Plant Safety and Compliance in Alberta

Learn more about how Edmonton Valve & Fitting field advisors can help you protect your plant and workers.

edmonton-Field Advisors TeamEstablishing and maintaining hydrogen plant safety is simple: prevent leaks throughout the entirety of a fluid system. This, of course, is about as helpful as setting operational efficiency benchmarks at 100%—easy in theory does not necessarily translate to easy (or even feasible) in practice. 

Some level of leakage can be an inescapable reality and sometimes an acceptable loss, especially when considering the size of the molecules involved in hydrogen production. That said, any efforts made to control and reduce leakage of the valuable fuel sources used in hydrogen facilities not only conserves product but will also reduce a plant’s fugitive emission levels. 

Reducing fugitive emissions offers a dual financial incentive, as evolving emission guidelines include more expensive fines or greenhouse gas offset credits. However, the greatest economic benefit of all is the protection of employees, equipment, and property. Without appropriate equipment and maintenance, hydrogen can readily escape to the atmosphere, where it can form a flammable mixture with the atmosphere in volumetric ratios around 4-5%. Hydrogen flames are exceptionally difficult to detect in broad daylight, and the low level of activation energy necessary for combustion means any hydrogen leak is nearly certain to result in a fire. 

The best way to prevent fires from leaked fuel sources is to prevent the leak in the first place. To do so, plants must leverage system components developed specifically for containing these molecules, a consistent approach to leak detection, and routine maintenance to identify leak points before they can develop further. 

In this guide, we discuss several common classes of components that have been meticulously designed and rigorously tested to meet the high demands of hydrogen plant safety. 

Regulators Provide Efficiency in a Leak-Tight Package

Regulators perform the crucial role of maintaining pressure across multiple system processes. They function as a tool of efficiency and stability, maintaining inlet and outlet pressures to surrounding components to ensure pressure optimization. As pressure regulators may operate with ratings up to 10,000 PSIG, the impermeability of the material is important. 

Hydrogen, with its small atomic and ionic size, can readily penetrate many surrounding materials, especially at elevated pressures. This leads to hydrogen embrittlement, where the ductility of the metal is reduced and becomes more vulnerable to fatigue and eventual crack proliferation. To prevent embrittlement, material selection for direct-contact materials is paramount. 

For relatively low-pressure concerns, an excellent stainless steel for this task is 316/316L, an austenitic alloy containing chromium, nickel, and molybdenum. The advantage of 316/316L (and other austenitic alloys) is the relative ductility and lower strain of austenitic to martensitic interstitial structures. An increase in ductility means an inherent reduction in brittleness, compounding the difficulty for hydrogen to diffuse into the metal. Further, the lower density of martensitic structures can form a pocket where hydrogen can continuously attack the metal. The family of RHPS pressure regulators have bodies built from 316L SS, which offers impressive corrosion resistance alongside the aforementioned hydrogen fatigue resilience to better reduce the incidence of leak point formation.

A diagnostic tool useful in leak detection of regulators is creep. Creep may be discerned when an increase in outlet pressure can be traced back to a seat leakage. Any otherwise unexplainable increases in outlet pressure should be a cause for investigation of the regulator seat by an operator. Certain designs, such as the self-centering poppet in the HF series, are better suited to handle the issue of creep. 

How Tube Fittings Interact to Make Better Seals

edmonton-tube-fittings-ferruleAs the juncture between the tubing and associated components, tube fittings can be an essential part of any plan to combat fugitive emissions. The mechanism that drives the function of the fitting is the sets of front and back ferrules. The ferrules collaborate to create tight seals and reduce vibration sensitivity by the act of first driving the front ferrules into the tubing while the back ferrules hinge inward for increased tube grip. By operating directly on the fitting body and indirectly on the outer diameter of the tubing, the front ferrules can create a two-stage seal. From there, the fitting can offer additional benefits to the tube’s operating conditions:

  • Gas-tight seal: Reduces fugitive emissions and allows for accurate measurements for system diagnostics, calibration, etc.
  • Vibration/tube grip: During assembly, the back ferrules protect against the induced stress riser. The colleting portion of the back ferrules creates more material contact, which acts to minimize bending at the contact point.
  • Thermal shock: The fitting compensates for changes in temperature during start-up and shutdown, minimizing thermal expansion/contraction and reducing expansion/contraction cycles serves to lengthen the product life of the tubing and reduce wear.
  • Installation: Torque is not transferred during the installation process, and repeat installations are predictable due to design specificity.

The surface finish of the tubing contributes greatly to the effectiveness of the seal created between it and the fitting. Defects incurred during installation or operation are likely to affect the ability of the seal to fully develop. To reduce the chances of failure at the seal, visually inspect and verify the surface is clean and free from nicks, scratches, or other surface abrasions that could inhibit seal formation. 

Multiple factors during installation can lead to improper seal function. To reduce the incidence of leaks, operators should be confident in their ability to perform essential operations on the tubing. Whether an operator is bending tubes, offsetting bends, retightening fittings, or using an inspection gauge, Edmonton Valve & Fitting offers training that provides users with the knowledge and resources to ensure their work is both safe and effective. With in-person and virtual training seminars available, Edmonton Valve & Fitting can furnish training that is tailored to the individual needs of any facility.

Hydrogen Plant Safety Begins With Valve Assessment

Valves are the largest contributor to fugitive emissions across an entire fluid system, with the vast majority of those emissions arising from failure at the valve stem. For any rising stem valves, such as needle valves, one component of controlling fugitive emissions is ascertaining that the product is certified low emissions by American Petroleum Institute’s 624 standard. The API test submits the product in question to a battery of mechanical and thermal cycles, and a product is only able to gain certification if methane leakage remains at or below 100 ppm for the entire duration. To further drive down emissions, the 1 Series Needle Valves, as well as the N Series Needle Valves, contain additional leak-preventative features.

1 Series N Series
2-piece chevron packing with disc springs to assist seal and reduce wear

316 stainless steel stem threads increase resistance to wear from cycling and prevent the formation of leak path via material degradation

Nonrotating ball stem tip provides reliable shutoff while preventing leaks

Seats have a maximum leak rate of 0.1 std cm3/s

 

The Alternative Fuel Service (AFS) Ball Valves are a great fit for any hydrogen plant. All wetted components in the assembly are compatible with both hydrogen and compressed natural gas, vastly increasing its utility to a hydrogen facility. Much like the needle valves, the AFS ball valves feature an API certification for low emissions under the 641 standard. The AFS achieves 641 certification with an ultra low-temperature fluorocarbon material in the O-ring compatible over the full temperature range of the valve as well as a seat-loading technology with excellent leak integrity for low- and high-pressure operations.

Metal Hoses Protect Your Service Lines, Insulation Protects Your Operators

As discussed above, the relative inertness between the 300 austenitic stainless steel alloys and hydrogen at low pressures makes metal tubing an indispensable piece of any hydrogen plant design. An internal helium leak test is conducted on all metal hoses, with an acceptable leakage rate seat at 1x10-5 std cm3/s. Product series such as the FX, FM, FJ, and FL possess a 316L stainless steel annular convoluted core and an additional 300 stainless steel alloy overbraid for pressure containment. 

For metal hoses integrated into temperature-dependent lines, insulation may be the most efficient option for temperature control. While their primary role is maintaining energy efficiency, insulation also assists in hydrogen plant safety in several key ways. First, the Safe-to-Touch ASTM C1055 standard establishes a max temperature of 60°C to protect operators from incidental contact; when in contact with a 60°C hose, no permanent damage should occur within the first five seconds. The air convection and flow about the tubing are also important to prevent a build-up of ice or condensation that could create a slip-and-fall hazard. To circumvent this issue, allow for adequate spacing between thermal lines (> 31 cm) and avoid routing through tightly confined areas with poor ventilation.

Orbital Welding: Saves Time and Protects Operators

Certain fluid system connections either require or benefit greatly by forming a permanent weld joint. Properly executed, a weld joint will form the least penetrable union possible, reducing the risk of leak development. While not viable in all circumstances, the ability to weld simple connections accurately and repeatably allows a facility to minimize downtime. An orbital welding unit and associated rigging offer the operator a high level of control over the weld puddle characteristics, and with a little training, can provide an indispensable tool in addressing simple welding jobs. A trained employee or welding professional with an orbital welding unit can enjoy multiple benefits relative to other welding systems: 

  • The operator can view weld puddle from an analytical perspective beyond eye evaluations. Sensors provide accurate measurements of temperature, current, arc, penetration, etc.
  • Since the weld is directly controlled by a computer interface, it is possible to reproduce welds to an extremely precise level. For repeatable jobs, time is saved after the initial job as settings will remain the same. With settings held constant, rework is also mitigated, which results in additional time savings.
  • Additional feasibility for welding in visibility conditions that would be dangerous or render a human welder ineffective.
  • The process of orbital welding is safer as no one has to be near the arc flash. Ergonomically, it can protect human welders from repetitive motion injuries or welding positions that are especially strenuous.
  • Orbital welding can accurately weld with or against gravity with accurate control of puddle variables. Though this is not beyond the skills of a professional welder, it may help alleviate time for rework, positional adjustment, etc.

Edmonton Valve & Fitting Can Make Sense of Leak Detection and Rectification

edmonton-leak-detection-rectificationEvery component throughout your fluid system plays a vital role no matter how big or small. For all these devices and their interfacings, fugitive emissions are an ever-present possibility. To best address leaks that may already exist in your lines and prevent future leak paths from forming, a consultation with an Edmonton Valve & Fitting Field Advisor can help maintain and develop your hydrogen plant safety. Keeping your valuable product where it’s intended to be so you can better serve your customers while protecting the health and wellness of your employees is something everyone can get behind.

 

To find out more about Edmonton Valve & Fitting can assess your system to minimize leakage and protect your operators, contact us through our website or by calling 780-437-0640
0213WeldingSystem-promo-1

Welding Systems

Swagelok welding systems can assist with the design and assembly of critical fluid systems.

More →

Field Advisory Services

Learn more about Field Advisory team and how they can help ensure the success of your pipelines. 

More →

View Locations

We serve northern and central Alberta from offices in Edmonton, Drayton Valley, and Fort McMurray.

More →

How can we help you today?

Whether you need a single component or help with complex systems, we are here to help.
Get in touch