Swagelok Tank Blanketing Pressure Regulators RHPS Series: Download the Catalogue

Swagelok’s new RHPS line of regulators includes tank blanketing regulators made of low-carbon stainless steel and factory tested with nitrogen or air at either 232 psig or its maximum rated pressure.

  • Types: pressure reducing and vapor recovery
  • 316L stainless steel construction
  • 1/2, 1, and 2 in. end connections
  • Working pressures up to 232 psig (16.0 bar)
  • Temperatures from –4 to 212°F (–20 to 100°C)

Which one is right for your job? Swagelok will be glad to help you make a selection. It doesn’t depend so much on the size of the tank as it does on filling and evacuation. A quarter-inch line on a 10,000 gallon tank will change the volume much more slowly than a four-inch line on a 100-gallon tank. Get an accurate read on how long it takes to fill or empty a tank on the line, and don’t make a “guestimate.” It’s surprising how often one person will guess five minutes, while someone else will guess 15 minutes for the same tank.

Fill the form to download the catalogue

Download this catalogue to learn about Swagelok's Tank Blanketing RHPS Series regulators. In a hurry or have a question? Please call 780-437-0640.

About us

Founded in 1965, Edmonton Valve & Fitting Inc. provides critical fluid system components to customers throughout Northern and Central Alberta. Contact us at 780-437-0640.

Download the Tank Blanketing Pressure RHPS Series Catalogue