Learn more about fugitive emissions, the root causes, and how to mitigate them.
Over the past several years, Alberta has passed regulations with the goal of reducing methane emissions by 45% by 2025. The requirements have been implemented gradually, but as deadlines approach and regulations come into effect, the pressure to cut fugitive emissions is increasing.
To reduce fugitive emissions, Alberta oil and gas companies need a strategy—but it doesn’t have to be complicated. By working closely with fluid handling experts to understand the root causes of fugitive emissions in your facility, you can select the right components to mitigate them.
Our local Field Advisors are some of the top industrial fluid consultants in central and northeast Alberta and are available 24x7 with On-Call Technical Support. Contact our team today to learn more.
To reduce fugitive emissions, Alberta oil and gas companies need a strategy—but it doesn’t have to be complicated.
The Alberta oil and gas industry loses billions of dollars every year to fugitive emissions.
Reducing methane fugitive emissions is a critical part of Alberta’s long-term strategy to combat climate change. However, this isn’t the only reason oil and gas companies should be interested in reducing their emissions. Reducing fugitive emissions has several immediate benefits:
Fugitive emissions reduction measures can pay for themselves in the long run by increasing efficiency and maximizing sellable methane gas. By implementing a plan to reduce fugitive emissions, Alberta oil and gas companies also demonstrate their commitment to stopping climate change while ensuring compliance with Alberta fugitive emissions regulations and protecting the environment.
Oil and gas processing plants contain thousands of valves, connections, and other components that can be potential sources of fugitive emissions.
Fugitive emissions from valves account for approximately 60% of all fugitive emissions in a typical oil and gas facility. Valves leak when they are improperly installed, damaged, loosened by vibration, or when they just wear out over time. If a valve is installed in the wrong orientation, it will leak, for example. Because oil and gas facilities contain thousands of valves, regular inspections are essential to identify and repair or replace them.
Any other place where multiple components join—for example, gauges, seals, instrument panels, rotating equipment, or seal support systems—is a potential leak point and source of fugitive emissions. If components are positioned where they are under a load, they can be damaged over time, leading to increased emissions and potential failure.
Vibrations from equipment can also cause fugitive emissions by loosening nearby connections over time. Any components or pipe connections near pumps, compressors, or other rotating equipment should be inspected frequently for loose connections.
Fugitive emissions come from gas handling components—so the best way to prevent fugitive emissions is to use high-quality components.
Valves are the first parts to upgrade in a fugitive emissions reduction plan. Aging valves can be replaced with modern valves with higher-quality metallurgy and improved engineering design. No matter what type of valve is being replaced, to minimize leaks, it’s important to select high-quality, fugitive emissions-compliant replacement valves. Fugitive emissions-compliant valves have been tested to the strictest industry standards to ensure their performance against leaks. For optimal protection against fugitive emissions, valves should be selected by or with the help of an expert who can determine the valve designs and materials that will best accommodate the process parameters at that location.
Fittings and connections—especially threaded connections—are potential leak points and should be regularly checked for fugitive emissions. Threaded connections should be eliminated wherever possible and replaced with flange connections or tube fittings. Bent tubing should be used rather than piping where appropriate to minimize the number of connections.
When selecting components to reduce fugitive emissions, be sure to consult a fluid systems expert who can help you choose the right design and materials for your application. They can also help you identify potential leak points and high-risk components that you may not have been aware of.
The Alberta oil and gas industry trusts Edmonton Valve & Fitting to provide advice and components to maximize your facility’s efficiency and reliability. Our expert Field Advisors can perform an onsite evaluation and recommend design and component upgrades to help reduce fugitive emissions in your facility.
Swagelok valves passed the American Petroleum Institute’s Low-E test for fugitive emissions without modification. By using Swagelok valves, you don’t just meet the strictest regulations in the industry, you exceed them. Most importantly, you ensure your people and equipment are protected by the most advanced components available.
To find out more about how Edmonton Valve & Fitting can help you reduce fugitive emissions with high-quality Swagelok valves, fittings, and other components, contact us through our website or by calling 780-437-0640.
From single components to complex fluid handling systems we have the products, expertise, and resources to meet your needs.
Learn more.
Edmonton Valve invites you to take advantage of Swagelok Field Advisory Services. Getting started creates no cost or obligation.
Get started today.
Edmonton Valve & Fitting Inc. services northern and central Alberta, Canada. Look for a location near you.
For 50 years Edmonton Valve has provided Swagelok products and expert support to companies in northern and central Alberta.
Click to see our entire line card.
Expand your knowledge with updates, tips, and resources crafted by one of our 65+ local experts. Subscribe now.
Proud member of the Canadian Council for Aboriginal Business since March 2022. We understand our responsibility towards supporting the interests of the aboriginal communities, and we are working towards establishing that.